NOTICE

Visualizations can be nested at any depth by means of ⮫ “Visualization Element: Frame ”, ⮫ “Introduction” . In order to use the “Switch to any visualization” frame selection type without any problems, a “Frame” must not contain more than 21 referenced visualizations.
You can reference other visualizations within a main visualization either in a “Frame” or a “Tabs” element, and then display them in the window pane of the element.
In the case of the “Frame” element, you can freely program which of the visualizations is displayed at which time. One option is to use the switch frame variable of the “Frame” element, which automatically triggers a switch according to its value. You can also program additional controls which, after user input, trigger input actions that result in switching a visualization.
Moreover, you can use the “Tabs” to reference visualizations. It is easy and advantageous that the “Tabs” element provides preconfigured control of the visualization switch.
For more information, see: ⮫ “Configuring User Inputs ”, ⮫ “Introduction”