Command: Add Visualelement Permalink

Function: The command opens a submenu containing all available visual elements as menu entries.

Requirement: You have configured the command in the “Customize” so that the command can be called from any menu.

When you select an element in the submenu, the element is added in the upper left corner of the visualization editor.