Symbol:
Function: Enables positioning assistance with snaplines
Call: Context menu
When inserting and moving elements, lines are shown which indicate where positions exist that match the positions of adjacent elements. In addition, lines are shown which subdivide the visualization editor into a grid.
This allows you to align elements with adjacent elements or arrange them in a fixed column and row layout.
You can adapt the command in the dialog. The minimum distance between elements and to the border is adjustable. You can also define a grid to easily align elements in a column and row layout.
If you press the [Alt] key while moving with the mouse, the support with snaplines is suppressed. No lines are displayed.