The dialog shows a list of all objects for which an automatic locking was not possible. In the optoins you define how CODESYS SVN will resolve the confilict.
|
These options are displayed if another user has locked the object. |
|
These options are displayed if there exists a more current version of the object on the server. |
|
These options are displayed if no connection can be established to the server. |
|
“SVN Project Settings” |
Opens the SVN project settings dialog (menu “Project Project Settings”). There you can change the settings for the automatic locking. |
|
“SVN Settings” |
Opens the general SVN project settings dialog (menu “Tools Options”). |