Command 'Ignore on commit'Permalink

Function: This command identifies an object and adds it to the "ignore-on-commit” list. Then it is deactivated in the commit dialog by default.

Call: Menu bar: “SVN”

Requirement: At least one object is available that is not in the change list ‎ignore-on-comment‎.

Objects of the "ignore-on-commit” list are overlaid with the _svn_icon_status_ignored symbol in the object tree. By default, they are not selected in the commit dialog, unless a dependency of a selected object requires it. These objects can always be selected manually in the dialog.