Function: This command opens the “CODESYS” dialog. In this dialog, define the caches that will be deleted.
Call: Menu bar: “Project SVN”.
Dialog 'CODESYS'
The authentication memory contains the authentication data of all SVN repositories for which the user has selected for saving the authorization data. This memory is deleted completely by this command. |
|
“Clear the shared on-disk cache.” |
|
“Clear the RAM cache of this instance.” |
|
The authentication data saved on the computer is stored in %APPDATA%\Subversion\auth
. This memory path is also used for most other Subversion client applications (for
example, TortoiseSVN and AnkhSVN). Therefore, deleting the authentication data affects
these applications as well.