Function: This command opens the “CODESYS” dialog. In this dialog, define the caches that will be deleted.
Call: Menu bar: “Project SVN”.
Dialog 'CODESYS'
|
The authentication memory contains the authentication data of all SVN repositories for which the user has selected for saving the authorization data. This memory is deleted completely by this command. |
|
|
“Clear the shared on-disk cache.” |
|
|
“Clear the RAM cache of this instance.” |
|
The authentication data saved on the computer is stored in %APPDATA%\Subversion\auth. This memory path is also used for most other Subversion client applications (for
example, TortoiseSVN and AnkhSVN). Therefore, deleting the authentication data affects
these applications as well.
: The data saved on the computer is deleted.