Command 'Get lock'Permalink

Symbol: _svn_icon_lock_acquire

Function: This command locks the object explicitly for you. The “Lock Message” dialog opens for this purpose.

Call: Context menu: “SVN”

Requirement: The versioned object is not locked (not overlaid with the _svn_icon_status_locked symbol).

Dialog 'Lock Message'

“Enter the reason why you lock the object:”

Lock message

Example: ‎Locked for processing task 123‎

Button “Recent Message”

Shows message in the dialog that have already been used. There you select one in order to use the lock message.

“Recursive”

_cds_icon_option_activated: The object is locked with all subordinate child objects.

“OK”

Locks the object

When the lock is successful, the object (in the object tree) is overlaid with the _svn_icon_status_locked symbol.