Module – General Permalink

Object: PROFINET Module

Table 492: Module Information

“ID number”

Identification of the module (from the device description).

“Slot number”

Position of the I/O module below the I/O device, starting at "1" for the first module and incremented for each additional module. This results automatically from the current structure in the device tree.

Table 493: User Parameters

“Set All Default Values”

CODESYS resets all settings to default values (see the "Default Value" column) from the GSDML file.

“Read All Values”

CODESYS reads the current values from the device and updates them in the editor.

“Write All Values”

CODESYS writes the current values from the editor to the I/O module. Not all I/O modules support parameter updates in run mode. If not, then an error message is displayed.