Tab: Ethernet/IP Local Adapter – Tags Permalink

The tab of the device configurator is used for communication between an Ethernet/IP Scanner and an Ethernet/IP Adapter. The tab shows all device connections from the device description. The user can define a connection tag for each of these device connections.

No additional connections can be added on this tab.

Requirement: This tab is displayed only if the device description contains the parameter ‎ShowTagsPage‎ and the value of the parameter is set to ‎TRUE‎.

Table with the device connections defined in the device description.

“Connection Name”

Information originates from the device description

Not editable

“Transport Type”:

Information originates from the device description

Not editable

“Connection Path”

Information originates from the device description

Not editable

“Symbolic Connection Tag”

Connection tag for the connection predefined in the device description.

Specified by the user.