The tab in the device editor of the EtherNet/IP adapter contains the basic settings for network communication.
|
IP address |
Address for the identification of the EtherNet/IP adapter device. |
|
Bootstrap Protocol This option is available only for adapters under the NetX scanner. |
|
|
MAC address |
Device-specific MAC address of the slave. |
|
Save IP address |
|
|
Compatibility check |
If the check fails, then an I/O connection is not established to the device and an error message is issued to the status page. |
|
Restore Default Values |
For generic devices only. |
: The address of the slave is saved. The requirement, however, is that the slave supports
this function. This option is only available for the CIFX scanner.
: The adapter uses its own keying values to perform an exact check of the keying values
from the EDS file. The user decides which keying information should be checked.