The tab provides another more detailed view of the process data, which is also displayed in the “Process Data” dialog. Moreover, the download of the PDO assignment and the PDO configuration is enabled here.
Requirement: The expert settings for the slave are selected.
|
List of the Sync Managers with data size and PDO type |
|
List of the PDOs assigned to the selected “Sync-Manager”. |
|
|
When a check box is selected, the PDOs are enabled and I/O channels are created. This is similar to the simple PDO configuration view. |
|
List of the PDOs assigned to the selected “Sync-Manager”. |
|
|
You can add new entries or edit or delete existing entries by executing the respective commands (“Add”, “Delete”, “Edit”) in the command bar or context menu. |
|
“Name” |
|
|
“Index” |
|
|
“Direction” |
|
|
“Flags” |
|
|
“Exclude PDOs” |
It is possible to define an exclusion list. When a PDO is enabled in the “PDO assignment”, others are disabled and cannot be enabled. |
|
“Sync unit” |
ID of the Sync Manager to which the PDO is to be assigned |
|
Displays the contents of the PDOs selected in the “PDO list”. You can add new entries or edit or delete existing entries by executing the respective commands (“Add”, “Delete”, “Edit”) in the command bar or context menu. You can change the PDO order by clicking “Move Up” and “Move Down”. |
|
“PDO assignment” |
|
|
“PDO configuration” |
|
|
“Load PDO info from the device” |
The current PDO configuration is read from the slave and entered into the configuration. The lists in the upper and lower right are then deleted and filled with the read data. This is especially useful when the ESI file is incomplete and the configuration is available only on the slave. |
: The PDO is transmitted from the master to the slave.