The tab contains the slave parameters defined in the device description file.
When the auto-configuration mode of the master is enabled, the parameters are configured here automatically according to the device description file and the network topology. For standard applications, manual modification is generally not required.
|
“Value” |
Only a few parameters are editable. Changes become effective only when the auto-configuration mode is disabled. Modifications should be avoided, as invalid settings may prevent the slave from reaching the operational state. |