Configuring a Task-Dependent Recording Permalink

You can configure a database on the runtime system and the data buffering.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

Timeout for trend recording

During a trend recording, it can happen that the application task triggers a timeout that is caught with an exception when transitioning from “Running” to “Stop”. Causes can be that file operations with the SQLite database are taking too long or that too many variables are being recorded. This usually happens on a target device with weak performance.

You can avoid the occurrence of an exception:

  • Configure the trend recording with less memory demand so that the amount of data that is stored is adapted to the target system.

  • Reduce the number of variables.