Command: Zoom into Macro Permalink

Symbol: _cds_icon_sfc_zoom_into_macro.png

Function: The command opens a macro for editing in the macro editor.

Call: “SFC” menu

Requirement: A macro is selected.

With the command, closes the main view of the SFC editor and opens the macro editor. This is also an SFC editor for editing the section of the SFC chart which is displayed as a macro box in the main view.

Click ⮫ Zoom out of Macro to return to the main view.