Command: Insert Step-Transition Permalink

Symbol: _cds_icon_sfc_insert_step_transition.png

Function: The command inserts a step and a transition before the selected position.

Call: “SFC” menu

If you have selected a step, then CODESYS inserts a new step-transition combination. If you have selected a transition, then a new transition-step combination is inserted.

The new step is named ‎Step<n>‎, where ‎n‎ is an incremental number starting at ‎0‎ for the first step that is inserted in addition to the initial step. The new transition is named ‎Trans<n>‎ by default. You can click the name to directly edit the default names.

For more information, see: ⮫ “SFC Elements: Step and Transition ”