Adding a macro Permalink

  1. Select the ‎Step1‎ step.

  2. Click “SFC  Insert Macro After”.

    The ‎Macro0‎ macro is inserted after the ‎Step1‎ step.

  3. Double-click the ‎Macro0‎ element.

    The macro opens in the implementation section of the editor. The name ‎Macro0‎ is displayed in the caption.

  4. Click “SFC  Insert Step-Transition”.

    A step-transition combination is inserted.

  5. Click “AS  Zoom out of Macro”.

    The implementation section returns to the main diagram.

For more information, see: ⮫ “SFC Element: Macro ”