Adding an association Permalink

  1. Select the ‎Step2‎ step.

  2. Click “SFC  Insert Action Association”.

    CODESYS inserts an association to the right of the ‎Step2‎ step.

  3. Click in the left field of the association to select the ⮫ qualifier.

    You can enter the qualifier manually or use the _cds_icon_button_threedots.png Input Assistant. Select ‎P‎.

  4. Click in the right field of the association to select the action.

    You can type the action or select it by using the _cds_icon_button_threedots.png Input Assistant .

    _cds_img_sfc_action_association.png