Option: --signaturethumbprint (thumbprint of the certificate which is used for signing compiled libraries) Permalink

If you add this option after the option ‎--project="<path of project file>"‎, then the project is opened and the thumbprint of the certificate for signing compiled libraries is passed.

Syntax:

--signaturethumbprint="<thumbprint of digital signature>"

Example

Automation Builder.exe --project="D:\projects\test.project" signaturethumbprint="3E96C9B61010CBDC3186021A1CAA64946DDCAAF3"