CODESYS is started directly with the specified profile. When you start CODESYS without this option, the “Select Profile” opens.
Syntax:
--profile="<profile name>"
<profile name>: You have to specify the profile name exactly as it is displayed in the “Help About” splash screen of the development system or in the start menu on your computer.
Example
Automation Builder.exe --culture=de --profile="Automation Builder 3.5"