Option: --ignorewhitespace (ignore whitespace in project comparison) Permalink

If you add this option after the option ‎--compare <project1> <project2>‎, then whitespace is ignored in the project comparison. Note that semantically relevant spaces, for example in ‎STRING‎ literals, are still taken into account.

Syntax

--compare="<path of project file>" "<path of reference project file>" --ignorewhitespace="true"|"false"

Example

Automation Builder.exe --compare "D:\proj\project1.project" "D:\proj\project2.project" --ignorewhitespace="true"