|
Name |
Data Type |
Initialization |
Description |
|---|---|---|---|
|
|
|
0 |
Address of the variable Example: Note: For bit access of a variable |
|
|
|
0 |
Offset of the variable address (in bytes) Example: Note: If the variable is global, then the offset is relative to the beginning of the area. If the variable is a local variable in a function or method, then the offset is relative to the current stack frame. If the variable is a local variable in a function block, then the offset is relative to the function block instance. |
|
|
|
0 |
Memory area number Example: Means that the variable is not global in the memory, but relative to an instance or on the stack Note: The memory areas are device-dependent. |
|
|
|
0 |
Number of bits (in bytes) Example: Note: If the variable is not an integer data type, then: |
|
|
|
0 |
Memory size of the variable (in bits) Example: |
|
|
|
0 |
Bit address of the variable Requirement: The variable is located in the input memory area |
|
|
|
|
Data type class of the variable Example: Note: For user-defined data types or function block instances, |
|
|
|
‚‘ |
Date type name of the variable as Note: For user-defined data types, the function block name or the DUT name is output. Example: |
|
|
|
0 |
Number of array elements Requirement: The variable has the data type Example: |
|
|
|
|
Elementary basic data type of the array elements Requirement: The variable has the data type Example: |
|
|
|
0 |
Memory size of the array element (in bits) Requirement: The variable has the data type Example: |
|
|
|
|
Information about the memory area
Example: Note: The memory area configuration is device-dependent. |
|
|
|
‚‘ |
Variable name as Example: |
|
|
|
‚‘ |
Comment of the variable declaration Example: |