The IEC operator is used for the bitwise NOT of a bit operand.
When the respective input bit yields 0, the output bit also yields 1, and the other way around.
Permitted data types: BOOL, BYTE, WORD, DWORD, LWORD
Examples
Result in Var1: 2#0110_1100
ST
Var1 := NOT 2#1001_0011;
FBD