Object: Project Settings Permalink

Symbol: _cds_icon_project_settings.png

Function: The object contains the configuration of the project.

Call

  • “Project  Project Settings” menu

  • Double-click the object in the device tree

CODESYS saves the ⮫ project settings directly in the project. When you transfer a project to another system, for example, the “Project Settings” object is transferred with it. There is no need for a project archive.

The project settings are valid throughout the entire project and provide possible settings for various categories, such as “SFC” or “Users and Groups”. The available categories vary, depending on which software packages you have installed via the Package Manager.