Symbol:
The object is used to list the received ⮫ network variables, ⮫ network variables and display the information: network and transmit information and sender.
To add the object to an application, click “Add Object Network Variable List (Receiver)”.
The Network Variable List (Receiver) lists the received network variables. These received network variables, which were declared in the ⮫ Network Variable List (Sender) of another device or project. You cannot change the network variables in the object editor.
For more information, see:
The object editor consists of 2 sections:
-
Information about the sender and transfer log of the list
-
List of declarations of network variables
-
Dialog: Add Network Variable List (Receiver)