Within the implementation, a method can call itself, either directly by means of the
THIS pointer, or by means of a local variable for the assigned function block.
-
<return value variable> := <POU name> . <method name> ( <argument passing> );
Direct call of the relevant function block instance with the
THISpointer -
<return value variable> := <POU name> . <method name> ( <argument passing> );
Call by means of a local variable of the method that temporarily instantiates the relevant function block
A compiler warning is issued in the case of a recursive ⮫ call. If the method is provided with the pragma {attribute 'estimated-stack-usage' := '<estimated stack size in bytes>'}, then the compiler warning is suppressed.
For an implementation example, see the "Attribute: ⮫ 'estimated-stack-usage'" chapter.
To call methods recursively, it is not enough to specify only the method name. If only the method name is specified, then a compiler error is issued: “Program name, function or function block instance expected instead of”
-
See also: ⮫ THIS