Implementation Permalink

Optional

  • Access to function block instances or to program variables is allowed for the implementation of the method.

  • The ⮫ THIS pointer allows for access to its own function block instance. Therefore, the pointer is allowed only in methods that are assigned to a function block.

  • A method cannot access ⮫ VAR_TEMP variables of the function block.

  • A method can call itself recursively.

  • There is no implementation for interface methods

    ⮫ Interface methods can have declared input, output, and ‎VAR_IN_OUT‎ variables, but do not contain an implementation.