Tab 'Applications'Permalink

On this tab of the generic device editor you can see which applications exist on the device. Depending on the system you can delete the applications from the device or retrieve detailed information about the application.

“Applications on the PLC”

List of the applications found via “Refresh list” during the last scan of the control device.

“Delete”

“Delete All”

Deletes the application selected in the list or all listed applications on the controller

Note: If a safety controller is inserted below a PLC, then this command can permanently interrupt the communication links of the safety controller to other safety controllers (via safety network variables), to field devices, and to the development system. The safe field devices and the other safety controller can enter the safe state as a reaction. The connection to the development system is affected only in the case of a safety controller that is connected to the main controller via a fieldbus. For more information, refer to the section "Subordinate Safety Controller".

“Details”

Opens the dialog box “Details”. It displays information defined for the application on the “Information” tab of the dialog box “Properties”.

“Contents”

Requirement: The “Download the application info” option is activated in the “Properties” of the application object on the “Application generation options” tab. This causes information about the contents of the application to be additionally loaded to the PLC.

The “Contents” button opens a dialog box with additional information about the differences between the latest generated code and the application code that exists on the controller. The different modules are displayed in a comparison view.

“Refresh List”

The controller is scanned for applications and the list is refreshed accordingly

You can configure the commands “Remove Application from Device” and “Remove Applications from Device” by means of the dialog box form “Tools  Customize”. These commands correspond to the “Delete” and “Delete All” buttons.