Symbol:
Function: The dialog is used to configure the settings which make for easier coding.
Call: “Tools Options” command, “SmartCoding” category
|
“Declare unknown variables automatically (AutoDeclare)” |
In order for the AutoDeclare function to be available in the ST editor as well, the “Enable for ST editor” option also has to be selected. |
|
“Enable for ST editor” |
Requirement: The “Declare unknown variables automatically (AutoDeclare)” option is selected.
|
|
“Show all instance variables in input assistant” |
|
|
“Show symbols from system libraries in input assistant” |
System libraries are automatically inserted in the Library Manager and displayed in light gray.
|
|
“List components after typing a dot (.)” |
When you type a dot ( |
|
“List components immediately when typing” |
Requirement: The “List components after typing a dot (.)” option is selected.
|
|
“Insert with namespace” |
|
|
“Convert keywords to uppercase automatically (AutoFormat)” |
|
|
“Automatically list selection in cross reference view” |
|
|
“Underline Errors in the Editor” |
|
|
“Highlight symbols” |
|
|
“Max degree of parallelism” |
List box for the number of parallel threads which can be used for the precompile processing CODESYS detects the displayed number of threads from the number of CPU cores. This default number should be changed only in exceptional cases. |
: The
: The AutoDeclare function is not available in the ST editor.