Function: With this dialog, you define the icons of the menu commands.
Call: “Tools Customize” command, “Command Icons” tab
|
“Assign” |
Opens a dialog where you can select the new icon (*.ico) |
|
“Remove” |
Removes the custom icon The default icon is active again. |
|
“Reset” |
Resets all command icons to the default settings |
|
“Load” |
Loads the settings from a stored file (<file name>.opt.keyb) |
|
“Save” |
Saves the current settings to a file (<file name>.opt.keyb) |
For more information, see: ⮫ “Customizing Command Icons ”