NOTICE

Information can be lost when converting from larger data types to smaller data types.
CODESYS provides the following integer data types.
|
Type |
Lower limit |
Upper Limit |
Memory |
|---|---|---|---|
|
|
0 |
255 |
8 bits |
|
|
0 |
65535 |
16 bits |
|
|
0 |
4294967295 |
32-bit |
|
|
0 |
2-1 |
64 bits |
|
|
-128 |
127 |
8 bits |
|
|
0 |
255 |
8 bits |
|
|
-32768 |
32767 |
16 bits |
|
|
0 |
65535 |
16 bits |
|
|
-2147483648 |
2147483647 |
32-bit |
|
|
0 |
4294967295 |
32-bit |
|
|
-2 |
2-1 |
64 bits |
|
|
0 |
2-1 |
64 bits |
For more information, see: ⮫ “Constant: Numeric ”