A subrange type is a data type whose value range is a subset of a base type.
Syntax in the declaration:
<variabel name> : <integer type> ( <lower index limit> .. <upper index limit> )
|
|
Valid IEC identifier For more information, see: Rules and recommendations for ⮫ “Identifier Designation ”, ⮫ Further information |
|
|
Integer basic data type for the subrange
|
|
|
Constant for the lower limit of the area which has to be compatible with the basic data type The lower limit itself is included in this range. |
|
|
Constant for the upper limit of the area which has to be compatible with the basic data type The upper limit is also included in this range. |
Example
VAR
i : INT (-4095..4095);
ui : UINT (0..10000);
END_VAR
If you assign a value to a subrange type in the declaration or implementation part that is not within this range, then CODESYS issues an error message.
i:=5000 //Results in an error message
Note: In runtime mode, it is possible to monitor the range limits of a subrange type
by using the implicit monitoring functions CheckRangeSigned and CheckRangeUnsigned.
-
See also: ⮫ CheckRangeSigned, ⮫ CheckRangeSigned
-
See also: ⮫ CheckRangeUnsigned