Symbol:
The “OPC UA Information Model” object is added to the “Communication Manager” in the application. When added, an OPC UA publishing object
and below that an information model object
as a child object are also added.
In the “Add OPC UA Information Model” dialog, specify a name for the information model and select the OPC UA information model. The selection includes the OPC UA information models which are installed in the “OPC UA Information Model Repository”.
For more information see: ⮫ “Using OPC UA Information Models ”, ⮫ “Using OPC UA Information Models”
-
OPC UA information model editor
-
OPC UA publishing editor