Symbol:
Function: The command transmits the trace configuration on the controller to the assigned application, and starts the data sampling. The sampled data is transmitted back to the development system. The trace diagram shows the current samples and continues running.
Call: “Trace” menu; context menu
Requirement: The command is available when the assigned application is in online mode.
For more information, see: ⮫ “Control the Data Sampling ”