Command: Toggle Bookmark Permalink

Symbol: _cds_icon_bookmark_new.png

Keyboard shortcut: [Ctrl]+[F12]

Function: The command sets or removes a bookmark at the current position.

Call: “Edit  Bookmarks” menu

Requirement: A POU is open in the editor and the cursor is set at a line in the program.

For more information, see: ⮫ “Setting and Using Bookmarks ”