Function: The command halts the application where the error is located despite a programmed exception handling.
Call: The command is not available by default, but it can be configured in “Tools Customize”. The command is located on the “Command Icons” tab in the “Online” category.
Requirement: The application is in online mode and contains a programmed exception which handles
the __TRY and __CATCH operators.
If you have configured the command in the “Online” menu and you call it from there, then the active application is affected. Then the command can help you to detect errors.
For more information, see: ⮫ “Operator: __TRY, __CATCH, __FINALLY, __ENDTRY ” and ⮫ “Dialog: Customize: Menu ”