Command 'Set Active Application'Permalink

Function: This command sets the selected application as the active application.

Call: Main menu “Project”, or right-click the “Application” object.

Requirement: The project has at least two applications. The selected application is not active.

Online actions apply only to the active application. The name of an active application is displayed in bold typeface in the device tree.