Command 'Save Project and Install into Library Repository'Permalink

Function: this command saves the project as a library in the 'system' library repository.

Call: Main menu “File”.

With this command CODESYS saves the project as a library in the 'system' library repository. This is an extension to the saving of a project as a library file using the “Save Project as” command. The library is installed on the local system and is immediately available for insertion into a project.