Command 'Try to Reload Library'Permalink

Function: This command tries to reload the selected library.

Call: Main menu “Library”.

Requirement: A library is selected that failed to load.

If for any reason a library is not available in the defined repository location when a project is opened, CODESYS displays a corresponding error message. Once you have rectified the error, i.e. when the library is properly available again, you can reload the library with this command without having to leave the project.