Symbol:
Function: The command opens the “License Repository” dialog for viewing information about individual licenses.
Call: “Tools” menu
Requirement: CODESYS is in offline or online mode.
In the license repository, you find information from the central license server about licenses according to ticket number.
You can specify the ticket number(s) from the clipboard or import a text file.
|
<List of the ticket IDs imported to the repository for components subject to licensing> |
|
|
“Licenses” |
If you select an entry in the ticket list, then the name and status of the licensed components are displayed here.
On the right side of the dialog, you get information about the license: |
|
“Name”: Name of the product to be licensed “Item number”: Item number on the license server “Return allowed”: It is possible to have this license deactivated for it to be activated again on another system. “Can be activated”: You can get the license activated in the License Manager. “Number of activations”: Previous number of successful activations “Activation date”: Date of the current activation “Container-serial” “Firm codes” “Comment” |
|
“Import Tickets” |
The default dialog opens for searching the local file system. If you open a text file that includes one or more "tickets" with license numbers, then these are imported to the repository. Alternatively, you could also paste the numbers to the list from the clipboard. |
For more information, see: and ⮫ “Command: License Manager ”
: The license is available and valid.
: The license has been found, but it is invalid.
: The license was not found.