Command 'Insert Negated Contact Parallel (Below)'Permalink

Symbol: _cds_icon_negated_contact_parallel_below

Function: The command inserts a negated contact with lines in parallel with and below the selected element.

Call: Main menu “FBD/LD/IL”, context menu

Requirements: The LD editor is active. A line, a contact or a box is selected.

See also