Command 'Insert Contact in Parallel (Above)'Permalink

Symbol: _cds_icon_ld_contact_parallel; keyboard shortcut: [Ctrl]+[P]

Function: This command inserts a contact with lines in parallel with and above the selected element.

Call: Menu bar: “FBD/LD/IL”; context menu.

Requirements: The LD editor is active. A line, a contact or a box is selected.

You can program closed parallel branches in a LD network as short circuit evaluation (SCE) or OR constructs. SCE branches are displayed with double vertical lines, and OR branches with single lines. Refer to the help page for "Closed branches".

See also