Command 'Insert File as Text'Permalink

Function: This command copies the contents of a text file to the active editor as the current cursor position.

Call: The command is not in any menu by default. You can add it to a menu by using the dialog box from “Tools  Customize” (command category “Text Editor”).

Requirement: The file must have the extension ‎.txt‎. The command is available in a text editor only.

Many development environments and text processing applications provide the option of exporting code and text as a plain text file. This command can copy the contents of this file to the editor.

See also