Command 'Insert Device'Permalink

Function: Like the command “Add Device”, this command opens a dialog box “Insert Device” for the selection of a device object. This object is inserted in the device tree at the same level as the currently selected object.

Call: Context menu of a device object in the device tree.

Requirement: An object is selected in the device tree below which a device object can be inserted at the same level.