Command 'Go To Reference'Permalink

Symbol: _cds_icon_go_to_reference

Function: The command opens the declaration location of the variable that is referenced by the pointer currently in focus in online mode.

Call:

  • Context menu in the declaration part or implementation code

  • Menu bar: “Edit  Browse”

Requirement: Online mode. A POU is open in the editor and the cursor is at a pointer. The referenced variable is stored in static memory.

If the pointer does not point exactly to the beginning of the variable, then a corresponding message is displayed when you switch to the variable declaration.

See also