Function: The command enables and disables the flow control.
Call: “Debug” menu
Requirement: The application is in online mode.




NOTICE

An active flow control extends application runtime.
When the “Confirmed Online Mode” option is selected in the communication settings, a dialog prompt opens when switching on the flow control to cancel the operation if necessary.
When flow control is enabled, it is not possible to use breakpoints or to step through the program.
For more information, see: ⮫ “Flow Control ”