Command 'Update Parameters'Permalink

Function: This command enters changes to the declaration of the selected element in the diagram.

Call: Main menu “FBD/LD/IL”, context menu

Requirements: The FBD, LD or CFC editor is active. A box is selected. An extending change has been made to the declaration.

The command checks whether a box and its declaration in the declaration editor correspond. The change is accepted for the box only if the declaration was extended. Deletions and overwrites are not updated.

See also