Command 'Remove Unused FB Call Parameters'Permalink

Symbol: _cds_icon_remove_unused_fb_call_parameters

Function: This command deletes inputs and outputs of the selected box to which no variable and no value were assigned. However, the default inputs and outputs are always retained.

Call: Main menu “FBD/LD/IL”, context menu

Requirements: The FBD or LD editor is active. A box is selected. The box has interfaces to which no value is assigned.

See also