Command 'Insert Box with EN/ENO'Permalink

Symbol: cds_icon_insert_box_eneno, shortcut: [Ctrl] + [Shift ]+ [E]

Function: This command inserts a box with a boolean input “Enable” and a boolean output “Enable Out” at the end of the selected network.

Call: Main menu “FBD, LD, IL”, context menu

Requirements: the FBD, LD or IL editor is active. A network is selected, but no box is selected.

See also