Command 'Insert Assignment'Permalink

Symbol _cds_icon_fbd_assign, shortcut: [Ctrl] + [A]

Function: This command inserts an assignment in the FBD or LD editor.

Call: Main menu “FBD/LD/IL”, context menu

Requirements: The FBD, LD or IL editor is active. A network is selected, but no box is selected.

In IL an assignment is programmed via the operators ‎LD‎ and ‎ST‎.

See also